Key Design Considerations For Selecting Rf Antenna | Avnet Abacus

Display portlet menu

Key Design Considerations For Selecting Rf Antenna | Avnet Abacus

Display portlet menu

Key design considerations for selecting the right RF antenna

When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f


When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas for wireless electronic devices. Some design choices may already be constrained, based on the overall system design. Basic choices that a system designer may make include:

  • What frequencies (often determined by what wireless protocol – e.g., Wi-Fi, BlueTooth, Cellular, GPS, NFC etc.) are needed?
  • What modem / transmitter will be used?
  • How much power will be available for the system? (e.g., Impacts antenna choices and wireless performance)
  • How much data throughput / speed is needed?
  • How much efficiency (Antenna gain) is required?
  • Where does the antenna need to be and even potentially what orientation(s) will the device be for wireless operation (e.g., Mobile or fixed?)
  • Where will the antenna be located on the PCB? (e.g., Cabled to the PCB but inside or connected to the device? External to the device?)
  • How much flexibility exists with the overall system design to modify antenna choices (e.g., location, size, type, number of antennas in the system). For example, if an antenna is positioned too close to metal, an LCD, a battery or another device component, it may not work at all. However, if the antenna is a few millimeters away from those components, it may work fine.

Today, an overwhelming majority of antennas are not visible externally – either they are on the PCB or internally cabled to the device. The days of the external ‘walkie talkie’ antennas are distant memories when with most new wireless devices due to the efficiencies of RF electronics and the pervasiveness of wireless networks around us.

There are, of course, other considerations. Efficiency can vary by antenna type (e.g., monopole, dipole, slot, PIFA, panel, etc.) and today’s wireless devices employ many different antenna designs. That’s important because smartphones, wearable electronics, other wireless devices and the growing demand for broadband connectivity are driving the use of more cellular, Wi-Fi™ and Bluetooth® antennas. The Internet of Things (IoT) and machine-to-machine (M2M) technology are also leading to additional wireless deployments that are expected to increase productivity and efficiency while evaluating the measurement applications, quality control, decision-making and customer relationship management.

Applications for wireless devices are incredibly diverse, ranging from industrial applications to smart home devices and surveillance systems. Wi-Fi antennas are showing up on refrigerators, door bells and various other home appliances.
 

Choosing an antenna

When evaluating antennas for a wireless device, the first step is always to determine if a standard, off-the-shelf antenna is suitable. Off-the-shelf antennas offer a great advantage in terms of aiding in quick time to market. Being able to quickly identify, prototype, and measure one or more antennas for a system can assure that the right choice is made and quickly – reducing overall product risk. Additionally, because their cost is amortized over large production runs, standard antennas are typically the lowest-cost option. However, today’s device designs are more complex and compact, and device manufacturers are forcing more antennas into smaller and complex geometries surrounded by unfriendly materials and objects. There may be times, however, where a custom device may be the best or only option for the application.
 

The starting line

After the frequency or frequencies and basic wireless architecture parameters have been determined, device manufacturers typically begin the design process by selecting one or more appropriate standard antennas for evaluation, which are available for virtually every allocated frequency. Based on diverse manufacturing and RF technologies, standard antennas offer high performance and ease of integration for wireless applications in the industrial, consumer, medical and automotive markets, among others. Standard antennas can perform well for less cost and risk than a custom solution and offer shorter lead times for bringing wireless products to market.

Once the antenna is selected, engineered and mounted into the prototype device, ideally there is some testing for performance in an anechoic chamber. If the antenna does not work, then either the design is modified, or another antenna is tried.
 

Calling on custom

However, if a standard antenna does not work effectively, designers can utilize the design expertise of experienced antenna suppliers. The supplier may be able to customize an existing standard solution, providing the system designer with what they need, cost-effectively, and quicker than going through a ground up new design process, for a full custom antenna. Customizations of existing antennas may range from changing cable lengths or connectors on the antenna cables; to making small changes to the antenna pattern to ‘tune’ the antenna so, that it can match the performance need of the application.

The design process typically begins with the device manufacturer sharing a CAD model of the proposed product with the antenna supplier. Software is used to simulate antenna performance based on the properties of the device, the enclosure and any surrounding metal, measuring parameters such as return loss and efficiency. Based on that information, the supplier builds a prototype antenna to test it and then adjusts the design as needed.

For example, one custom project included a cellular antenna plated on the plastic device enclosure. A small number of prototypes were created and tested, and it was determined that they needed to be several millimeters shorter to compensate for the effect of the plastic enclosure. Using calipers and a sharp knife, the radiating arms were trimmed to the appropriate length based on the wavelength of the signal the device was designed to pick up. The tested, shortened antenna design went into full production.

There are many technologies that are used to produce custom antennas – one of the most common involves plating conductive antenna ‘traces’ on plastic and is called Laser Direct Structuring (LDS). LDS is used to make antennas in many 4G cell phones and other compact devices that could not support any other type of standard internal antennas. Generally, higher volumes are needed to justify the effort to use LDS and other custom antenna technologies.
 

Test, retest, and re-retest

Once selected and designed into the system, it is very smart to test to see how effective the antenna is. Antenna design is iterative in nature. This is true with both design of the actual antenna element and can be true even when designing in an off-the shelf antenna into a system. Ask RF engineers if changing a particular antenna parameter would improve the design and they will typically say “There’s no way to know. We have to test it.” In other areas of applied science, engineers might be willing to provide an educated guess to a similar question, but with RF, antenna sensitivity to surroundings and typically razor-tight performance margins make actual testing the product the only answer – then testing it again and again, if needed.

Designers never begin a device development project hoping it will require a custom design; standard off-the-shelf RF antenna solutions are always preferred due their lower cost and short lead times. However, when a custom antenna is needed, the design and testing resources of an experienced antenna supplier are vital in creating a solution that works effectively for today’s complex, often small wireless devices.

Finally, it is worth noting that with nearly all RF devices, some type of approval is required with the full system for release to commercialization. All the previously mentioned antenna testing is not only important to ensure adequate device performance and happy end users, but it may be necessary to get FCC approval for the device. In the event that the device is used in a cellular network, it will be necessary for the device to pass the requirements of all carrier RF requirements. Generally, the higher the speed of a device on a 4G network, the more demanding and challenging this certification process is – e.g., a Smartphone is required to go through more extensive testing and validation than a LTE enabled home surveillance base-station. Devices with well-designed antennas that have gone through iterative cycles of antenna performance testing, will fare through finished product RF validation and testing such as carrier or FCC testing.

In summary, the more attention that can be given to making smart antenna choices early in the design process, the better the wireless performance will be.

Wi-Fi and Bluetooth are trademarks or registered trademarks and are the property of their respective owners.

 

 

Written by 

Matt McWhinney

Matt McWhinney is a business development manager at Molex. Matt has a degree in electrical engineering, enjoys working with innovative customers and is a technology enthusiast of smart and power electronics.

Discover Molex's antenna solutions for Smart Home applications

Key Design Considerations For Selecting Rf Antenna | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

Key Design Considerations For Selecting Rf Antenna | Avnet Abacus

Display portlet menu
Related Articles
Automation manufacture Industry 4.0
Evolution before revolution: the origins of Industry 4.0
May 27, 2020
We’ve come a long way from the days of Henry Ford famously telling customers that they could have the Model T car painted any colour ‘so long as it was black’ – a quote which reflected the compromise of having to put efficiency before choice.
Product
The evolution of cellular networks
By Martin Keenan   -   April 29, 2020
Since the first 5G services were launched in the USA by Verizon and AT&T, 5G networks have been rolled out in a further 17 countries with South Korea, the United Kingdom, Germany, and the United States leading the charge and China catching up fast.
Autonomous vehicles communicating with each other on roads
How automotive Ethernet and 5G will power autonomous driving
September 22, 2020
Automotive Ethernet and high-performance 5G communication systems will form the backbone of autonomous vehicles, enabling safety, and increased comfort for drivers and passengers.
Abstract image of an electronic circuit
How SiC and GaN technology is affecting passive component development
June 19, 2020
To keep up with the semiconductor process innovations, SiC and GaN present some unique challenges to the essential passive components used in power conversion and motor drive circuits.
Satellite in action around the Earth
The future is 5G
By Adam Chidley   -   April 29, 2020
'The explosive growth of the IoT shows no signs of abating, with Gartner forecasting 20.8 billion connected “things” by 2020, and IHS Markit predicting that this number will rise to 125 billion by 2030.'
A technical specialist on solar panels
Extending battery lifetime in wireless applications using supercapacitors
By Martin Keenan   -   April 20, 2020
This article describes how supercapacitors can be deployed in conjunction with batteries to extend their operational life and reduce maintenance and replacement costs.
Engineer using an oscilloscope to test a circuit
Selecting relays for test and measurement equipment
By Shlomo Avital   -   March 30, 2020
Follow Avnet Abacus on LinkedIn  One of the key challenges with developing test and measurement equipment is to ensure that the signal that gets measured is the same as the signal that you want to measure. It sounds obvious, but multiple factors in the ...
An electric vehicle charging cable being plugged into a charging station
An introduction to EV charging infrastructure design
February 7, 2020
With demand for faster charging of EV vehicles increasing, the design of charging stations and infrastructure becomes ever more important.
Inside of a connected car depicting
V2X: The future of vehicle communications
By Martin Keenan   -   December 10, 2019
Vehicles are about to become a lot more communicative: with other road users, with the infrastructure they pass on their journeys, with cloud-based services, and even with the energy grid. This communication should make vehicles more economical to operate...
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
PIR and ultrasonic sensors: What's the difference and how do they work?
By Alessandro Mastellari   -   October 21, 2019
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
4 factors steering connector choices in today's automotive applications
September 16, 2019
Connectors are critical components in any automotive systems, and their selection can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
Industry 3.0 vs. Industry 4.0: Selecting connectors for the new industrial age
June 17, 2019
When specifying connectors for IIoT applications, making the right choice is vital to ensuring the integrity of the transmission. Vibration, humidity and environmental stress are regular concerns when specifying any system component for a factory or
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
A quick guide to multi-standard mesh networking
By Alessandro Mastellari   -   April 11, 2019
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Design trends: Automotive passives
By Martin Keenan   -   November 29, 2018
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
Selecting an Ethernet ICM the easy way
By Marco Enge   -   July 25, 2018
An ICM, or integrated connector module is a type of connector that integrates all the magnetics required to meet the Ethernet standard for xBASE-T connections. They provide a quick and easy solution for Ethernet connectivity, but how do you know whic
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
Wireless modules point the way for IoT connectivity
By Martin Keenan   -   June 26, 2018
You've selected your wireless protocol, and you're ready to start designing. But should you take the modular route or build a discrete solution?
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Future proofing lighting systems with Bluetooth
By Alessandro Mastellari   -   May 9, 2018
The lighting industry is not short of options for digital connectivity, but what it needs is a standard that adapts itself to change. Enter Bluetooth 5.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Optimising battery designs with supercapacitors
By Tim Parker   -   April 30, 2018
The role of the battery in product design has become increasingly important. In fact, you could say it has provoked a change in design methodology, albeit with a bit of help from legislative bodies.
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
From enabled to proactive: The evolution of home automation
March 29, 2018
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
Man controlling home devices via his watch
Let your home do the work so you don't have to
By Martin Keenan   -   March 29, 2018
Today, we need to interact with connected products in the home deliberately. But it does not have to stay this way.
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Adapting PIR sensor technology to new applications
By Martin Keenan   -   February 7, 2018
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
EV charging points set to rapidly increase in numbers
By Marco Enge   -   January 18, 2018
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Protecting outdoor electronics against vandals
By Jerry Moss   -   December 18, 2017
Electronics used in outdoor locations have to contend with harsh weather conditions, including direct sunlight, rain, ice, and even earthquakes. But that’s not the whole story.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
RF When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Advances and trends in RF connection
By Marco Enge   -   October 19, 2017
When considering the exponential growth of transferred data, most headlines are captured by wireless innovation, but advances continue to be made in the wired domain, not least in RF connectors.
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
Enabling smart tracking for the supply chain and Industry 4.0 with RFID
By Adam Chidley   -   September 27, 2017
Do you know where your product has been and where it is going right now? This is the challenge that many manufacturers and logistics companies face in the management of their supply chains, but how can RFID technology solve it?
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
How wireless power transfer can help make the world’s lithium go further
By Martin Keenan   -   September 19, 2017
As pressure on the world’s lithium reserves increases, wireless power transfer simplifies charging and enables designers to use lower-capacity batteries and create new types of smart devices.
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Weather, corrosion and vandals: Protecting outdoor electronics
By Jerry Moss   -   June 30, 2017
Specialised enclosures and switches are required for electronics’ survival in the great outdoors, writes Jerry Moss, Avnet Abacus.
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost.
Keeping the noise down: Converter and inverter output filtering
By Adam Chidley   -   May 31, 2017
Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Selecting DC-link capacitors in power converters
By Adam Chidley   -   May 10, 2017
‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance.
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Input filtering and protection for switched mode inverters and converters
By Adam Chidley   -   April 25, 2017
Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment
Datacentre racks
Chip-to-chip at the speed of light
By Marco Enge   -   March 31, 2017
As data centres and data farms continue to expand and grow, better solutions are required for system architectures that allow faster communication and more efficient operation.
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Specifying explosion-proof connectors
By Marco Enge   -   March 30, 2017
The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation.
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Hybrid capacitors combine technologies to get the best of both worlds
By Martin Keenan   -   March 15, 2017
Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries.
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
Understanding ESR in electrolytic capacitors
By Adam Chidley   -   March 1, 2017
Adam Chidley explains how component diversity has made selecting the best capacitors for power-related applications more complex than ever, and why taking independent advice makes sense.
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Ethernet magnetics – Discrete or integrated?
By Adam Chidley   -   July 29, 2016
If you’re adding wired Ethernet to a design, you will of course have to consider magnetics.
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Selecting fibre optic cables
By Marco Enge   -   July 12, 2016
Selecting the right cable and/or connector assembly for a fibre optic installation need not be complex, but it is important to understand the requirements of the environment and the application.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Calculating LED heatsinks
By Giovanna Monari   -   May 22, 2016
Thermal management is of critical importance in LED lighting systems. LEDs themselves give off heat when lit due to their own inefficiencies, and knock on effects of that heat can rapidly reduce the LEDs’ lifespan if it isn’t managed carefully.
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
‘Wet’ aluminium and polymer aluminium capacitors – what’s the difference?
By Ekaterina Rachel   -   April 1, 2016
Aluminium electrolytic and polymer wound aluminium electrolytic capacitors may seem similar at first glance, but the technologies offer very different performance characteristics.
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
Modern electromechanical relays meet today’s reliability demands
By Giovanna Monari   -   February 2, 2016
Although they’ve been superseded in some applications by newer technologies such as solid state relays (SSRs), electromechanical relays (EMRs) still have a lot to offer.
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Circuit protection is vital for long lifetimes in LED lighting
By Adam Chidley   -   January 7, 2016
LEDs are widely touted as the perfect solution for lighting applications because, in theory at least, they last forever.What’s less frequently spoken about is that circuit protection can make or break the design.
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
Supercapacitors: Making transport more efficient
By Adam Chidley   -   September 7, 2015
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The unstoppable rise of polymer capacitors
By Ekaterina Rachel   -   August 10, 2015
The various types of capacitors all have their advantages and disadvantages, but polymer capacitors offer a host of desirable electrical characteristics.
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Understanding micro switches and hysteresis
By Giovanna Monari   -   June 12, 2015
The invention of the micro switch goes back over 80 years to 1932 and is attributed to one Peter McGall of Freeport, Illinois, USA. Who knows how many billion of these handy little components have been manufactured since, but there can hardly be a ho
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Fans have few fans, but perhaps they should?
By Mathias Goebel   -   May 28, 2015
Fans are often looked at like insurance policies – they’re something you need, rather than something you want.
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
What’s super about supercapacitors?
By Adam Chidley   -   May 18, 2015
Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications.
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
Latest developments in antennas for M2M communications
By Marco Enge   -   April 30, 2015
Machine-to-machine (M2M) communications has undergone phenomenal growth in recent years and connectivity is becoming increasingly reliant upon wireless networks.
A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality.
How sensitivity to our environment is creating a growing market for air quality sensors
By Giovanna Monari   -   April 2, 2015
A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality.
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.
LED thermal management: Is it just me or is it getting hot in here?
By Giovanna Monari   -   March 19, 2015
Thermal management is a key element of LED lighting design, ensuring reliable operation, better performance and extended device lifetimes.

Key Design Considerations For Selecting Rf Antenna | Avnet Abacus

Display portlet menu
Related Events