The Growing Market For Air Quality Sensors | Engineers' Insight | Avnet Abacus

Display portlet menu

The Growing Market For Air Quality Sensors | Engineers' Insight | Avnet Abacus

Display portlet menu

How sensitivity to our environment is creating a growing market for air quality sensors

Giovanna Monari Photo

A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality.

A growing pre-occupation with leading healthier life styles means that many of us are becoming much more sensitive to the environment around us, and in particular air quality. There’s even a London web site dedicated to providing information about air pollution in the city and of course and inevitable smartphone app to keep you up to date with the facts on how quickly you’re being poisoned. Yes, air pollution and mortality rate are closely linked. Public Health England (PHE) published a report in April 2014 that estimated the number of deaths in UK local authorities attributable to long term exposure to man-made particles less than 2.5 microns in diameter. It concluded that 8% of deaths in London (and possibly almost double this number) could be attributed to long-term exposure to particulate pollution – most of which is created by motor vehicles. All cities suffer from this kind of pollution, some more than others, depending on traffic density, other sources of particulates, weather conditions and various geographic factors.

However, particulates are not the only pollutants that damage health. Carbon monoxide (CO), excess levels of carbon dioxide (CO2), and high concentrations of gases such as propane or methane also have adverse, and sometimes fatal consequences for humans. 

Some air conditioners in offices and homes no longer just operate on the basis of controlling temperature. Smart sensors also take account of humidity, particulates of various sizes and even the presence of tobacco smoke.

One US company, Sensorcon, developed a multi-sensor tool, called Sensodrone, for use with a smartphone. Funded through KickStarter, the firm describes the product as “the world’s first mobile, wearable, programmable sensing computer” and one journalist described it as “a Swiss Army Knife of environmental input.” 

Sensodrone incorporates a carbon monoxide detector, non-contact thermometer, gas leak detector, lux meter, weather station, diagnostic tool, breath analyser and more. 

 

The much-vaunted Internet of Things will involve billions of sensors from which data is processed and communicated, and new products that control and safeguard our environment will be developed in their droves over the next few years. Here are just a few examples of CO2, humidity and temperature sensors.

Amphenol air quality sensors include The Telaire T6613/66715 series of modules for CO2 detection (right). They come in single and dual channel versions and there are complementary duct-mount or wall-mount transmitters. Humidity and temperature models of the wall-mount versions are available too. Accurate sensing results in well-controlled environments in which energy consumption is minimised, realising considerable cost savings.

Alps humidity sensors are used in everything from home appliances to health care devices. Various versions provide absolute or relative humidity measurement based upon changes in the mechanical or electrical state of hygroscopic materials inside the devices. The most popular type, the HSHCA, translates changes in humidity to changes in capacitance to produce a highly linear response without the need for temperature compensation circuits. The Alps HTUD sensor is a plug-and-play device that combines humidity and temperature sensing in one compact, DFN package.

Amphenol EMD-4000 sensors are resistive devices for measuring relative humidity. They’re used in air conditioning systems for commercial premises, homes and automobiles and have a measurement range of 20% to 95% relative humidity at 25 °C.

TDK also uses resistive humidity sensing in its CHS family of humidity sensors. The products are particularly resistant to the ingress of water and various gases, and exhibit no hysteresis when measuring between 5% and 95% relatively humidity levels.

   

Hygrometers and air humidifiers are the primary applications for capacitive atmospheric humidity sensors from Vishay. Each sensor consists of a non-conductive foil, which is covered on both sides with a layer of gold. The dielectric constant of the foil changes as a function of the relative humidity of the ambient atmosphere and, accordingly, the capacitance value of the sensor is a measure of relative humidity. Relative humidity from 10% to 90% is measured and the devices can be used from 0 to 85 °C, a wider temperature range than most of the resistive types.

Humidity sensors and humidity/temperature sensor modules (left) are also made by TE Connectivity (formerly Measurement Specialties). These sensors employ a unique capacitive cell for humidity measurement and a Negative Temperature Coefficient (NTC) thermistor for temperature measurement. They’re useful in applications where dew point, absolute humidity measurements or humidity compensation are required. 

 

 

These are just a few examples of sensors available from Avnet Abacus. If you need help in selecting the best one for your application, please get in touch using our Ask an Expert page.

Want more like this? Sign up for our newsletters

About Author

Giovanna Monari Photo
Giovanna Monari

As a Senior Product Manager, Giovanna is responsible for marketing strategy and supplier management ...

The Growing Market For Air Quality Sensors | Engineers' Insight | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

The Growing Market For Air Quality Sensors | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Articles
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
Taking flow measurement to the next level
By Alan Jermyn   -   October 25, 2019
Avnet Abacus helps engineers to develop smart flow meters for monitoring water and gas consumption. Alan Jermyn, VP Marketing, looks at what’s driving demand for smart meters, how they work and how they’re built.
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
PIR and ultrasonic sensors: What's the difference and how do they work?
By Alessandro Mastellari   -   October 21, 2019
There are two primary technologies used in detecting the presence of people, pyro-electric / passive infra-red (PIR) and ultrasonic. Alessandro Mastellari takes a look at how they differ and how they work.
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
Maximise your IIoT installation success by choosing the right sensors
July 19, 2019
How are the latest trends in sensing technology enabling the Industrial IoT, and how do you make the right choice for your installation?
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
A quick guide to multi-standard mesh networking
By Alessandro Mastellari   -   April 11, 2019
Recent advances in wireless technology have enabled the use of mesh network topologies in home and building control applications, but what are your options, and can you combine them?
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering
Women in engineering – where are we now?
By Lisa Rees   -   March 7, 2019
To mark International Women’s Day, we spoke to two female engineers at different points in their careers – one from the UK and one from Germany – to find out from them what their take is on being a woman in engineering and to learn more about t
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
A quick guide to powering smart objects with kinetic energy harvesting
By Alessandro Mastellari   -   January 22, 2019
As the world becomes increasingly smart and connected, batteries can be undesirable in some of the use cases. Kinetic energy harvesting is an alternative that can help achieve longer operating lifetimes, relieve ownership costs, and ideally improve r
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica
November 16, 2018
And so electronica 2018 is over. In our final post, we look back on the best bits of day three.
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
electronica 2018 day two highlights
November 15, 2018
Another day at electronica 2018 has passed and it was arguably even busier than the first. A constant stream of customers and suppliers kept the atmosphere on the Avnet Abacus stand buzzing, and our schedule was packed full of great speakers and demo
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
electronica 2018 day one highlights
November 13, 2018
On a crisp morning at Messe Munich there was an excited buzz around the exhibition centre as electronica 2018 opened its doors. Read what happened on day one.
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
Key design considerations for selecting the right RF antenna
August 7, 2018
When faced with the need to make design decisions, system engineers are challenged with multiple options, any of which can have a major impact on the effectiveness of the wireless performance.There are many considerations when selecting RF antennas f
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Security and surveillance: Two sides of the coin in smart homes
By Martin Keenan   -   July 9, 2018
The new era of home security won’t just be an alarm that rings when a lock is picked or a window broken. With the rise of new technology comes the added need to protect a home’s hardware and its software.
Wireless technology is endemic in modern society; broadly speaking we rely on cellular technology to stay connected when we’re travelling, and probably WiFi when we’re not.
Choosing the right wireless technology for your IoT end-device
By Adam Chidley   -   May 4, 2018
Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-Fi access point to your home broadband. Avnet Abacus’ Adam Chidley takes a look at low power WANs and why they will be essential in connecting thin
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
From enabled to proactive: The evolution of home automation
March 29, 2018
Just how smart can a smart home get? Tomorrow’s home is a true a brainiac, making decisions for you before you even think to tell it to.
Man controlling home devices via his watch
Let your home do the work so you don't have to
By Martin Keenan   -   March 29, 2018
Today, we need to interact with connected products in the home deliberately. But it does not have to stay this way.
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Adapting PIR sensor technology to new applications
By Martin Keenan   -   February 7, 2018
The passive infrared sensor (PIR) seems so familiar that it is easy to miss the many applications that exist for it and the subtleties of engineering that guide the best ways in which to use it.
Giving machines the power of vision gives them the ability to interact with people in a much more natural way, but integrating this capability was previously a complex and difficult task.
I recognise that face: Machine vision with Omron's HVC
By Giovanna Monari   -   November 14, 2017
Giving machines the power of vision gives them the ability to interact with people in a much more natural way, but integrating this capability was previously a complex and difficult task.
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Customising and optimising antennas with materials science and manufacturing techniques
By Martin Keenan   -   July 14, 2017
In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a t
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
Evolving component technologies will make Industry 4.0 viable
By Martin Keenan   -   May 22, 2016
Industry 4.0 and the digitisation of the manufacturing sector will have repercussions for all sectors of industrial electronics.
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
The internet of medical things (IoMT) bringing better healthcare for all
By Martin Keenan   -   April 8, 2016
The Internet of Things (IoT) combines pervasive connectivity to control devices remotely with Big Data applications in The Cloud capable of organising vast quantities of information and extracting information hidden in the data to enable new services
How can MEMS pressure sensors help you keep fit? Well, they are now commonly being integrated into wearable activity monitors that help consumers track their daily activities and thereby monitor their fitness levels.
Accurate altitude measurements help keep you fit
By Mathias Goebel   -   October 20, 2015
How can MEMS pressure sensors help you keep fit? Well, they are now commonly being integrated into wearable activity monitors that help consumers track their daily activities and thereby monitor their fitness levels.

The Growing Market For Air Quality Sensors | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Events