The Shift to 48V in Automotive Systems: What You Need To Know | Engineers' Insight | Avnet Abacus

Display portlet menu

The Shift to 48V in Automotive Systems: What You Need To Know | Engineers' Insight | Avnet Abacus

Display portlet menu

The shift to 48V in automotive systems: What you need to know

The complex electronic architectures of  hybrid and electric vehicles have required engineers to rethink power requirements. Here's why 48V DC systems are key to modern automotive systems, and some considerations on powertrain component selection.

One of the biggest current trends in car design is the shift to hybrid and fully electric vehicles. Less obvious to the public, perhaps, is a fundamental change in the architecture of vehicles’ electrical systems, with the introduction of 48V DC systems to work alongside the 12V DC systems we have used for decades. But what is driving this change, and what will it mean for companies developing vehicle electronics, and the component suppliers that serve them?
 

Power play

It’s here that your high-school physics lessons prove their value. Remember ‘watts equals volts times amps’? This handy equation tells us that you can deliver the same power electrically using either high voltages and low currents, or high currents and low voltages. A second equation, ‘watts equals current squared times resistance’, tells us that it makes sense to deliver power at high voltages and low currents, to minimise resistive losses.

This is one of the key reasons for a shift to 48V: modern cars, their energy-hungry climate-control, powerful driver-assistance computers, and complex infotainment systems together mean that cars now consume much more electrical energy than they used to. It makes sense, therefore, to shift to 48V to minimise resistive losses. The shift to 48V also allows higher currents, and therefore greater power delivery, so features such as window demisters and heated seats can be more effective by working more quickly.

These may seem like trivial reasons for making such a substantial change to a system that has served us well for decades, but they sell cars – some US truck makers are promoting their use of 48V systems by pointing out that they will enable users to run power tools from their vehicles. Potentially much more important, adding 48V systems will enable hybridisation, bringing greater fuel economy and reduced emissions to vehicles at relatively low cost.
 

The shift to hybrids

2019 Dodge Ram 1500 pick up truck parked on a hill in a forest

The 2019 Dodge Ram 1500 pickup uses a mild
hybrid configuration tocut fuel consumptions
(Image credit: shutterstock.com)

 

The first step towards hybridisation is to use 48V systems to help run internal combustion engines more efficiently, by driving auxiliary functions such as power steering racks, brake vacuum pumps and water pumps with electric motors rather than using a power take-off from the engine. This can be more energy efficient than mechanical drive, since the operation of these functions can be more closely matched to the vehicle’s needs. For example, intermittent electrical drive is more efficient than continuous mechanical drive for running vehicle air conditioning, because an AC system’s compressor is off more often than it is on.

The next step is a ’mild hybrid’, which replaces a car’s traditional starter motor with a motor generator unit (also known as a belt-driven starter generator). This acts as generator under braking, recharging the vehicle’s battery. When the vehicle comes to a stop, the motor generator, driven by AC power provided though an inverter from the battery, can restart the internal combustion engine and set the vehicle moving again more quickly by providing additional torque. Industry estimates say this approach can improve fuel economy by 10 to 20% at a much lower cost than a full hybrid approach.

Using a slightly more powerful motor generator will enable a car to creep through a parking lot or a city’s low-emission zone on electric power, reducing fuel consumption and emissions. More complex hybrids use much more powerful motors to handle traction at normal road speeds. They also use the electric motor to smooth out torque delivery from the internal combustion engine, when changing gears or pulling away from a stop, and to provide additional power as necessary. These two strategies help keep the engine operating at its peak efficiency, reducing emissions and making the vehicle more responsive and fun to drive.
 

Making the transition

The industry has too much invested in 12V electrical systems to try to make an overnight transition to 48V. Instead, the shift to 48V will come gradually, with the introduction of 48V infrastructure to run alongside the ‘legacy’ 12V system. A generic 48V system is likely to include a 48V battery and battery controller, the motor generator unit and inverter, power bus and connection points, as well as a DC/DC converter to transfer power between the two systems as needed.

Shifting to 48V will demand the development of a wide range of new componentry that can operate at this higher voltage and meet the demanding standards of the automotive industry. For example, mild hybrids will need efficient inverter circuits to be able to contribute energy to, and draw energy from, the onboard 48V battery without excessive losses. Wiring looms may have to be upgraded to handle the higher voltages and currents, as will any devices that are switching significant amounts of power at 48V.

 

Eaton XLR series 48V supercapacitor

Eaton's 48V supercapacitor can provide short bursts of high power

We’ve already talked about using electric power to fill gaps in an internal combustion engine’s power curve, or just to provide a boost. In most cases the energy for this will be drawn from a battery, but there is an alternative approach: a super-capacitor. Eaton offers an XLR 48V super-capacitor module (right) designed for high power, frequent charge/discharge systems in hybrid or electric vehicles, public transportation, and related applications. Eaton argues that adding such a model to a hybrid can reduce battery size and weight or even replace batteries altogether in some cases. The 166F, 5milliohm module is made up of 18 supercapacitor cells, and includes cell-voltage management circuitry and an over-voltage alarm. It’s sealed to IP65, making it suitable for use in dusty areas and where it will be jet washed.

You should also expect rapid development in power electronics to serve the opportunity created by the shift to 48V systems.

One key area will be charging control and battery management. Companies such as NXP are already producing relevant battery-management devices, such as the MC33771B Li-ion battery manager for up to 14 battery cells with built-in current balancing.

Efficient DC/DC conversion is also important. ON Semiconductor has developed highly integrated modules, such as its FTCO3V85A, an 80V, low Rds(on) automotive-qualified power module featuring a three-phase MOSFET module, for use in 48V DC/DC conversion.

Vendors are also exploring multiple approaches to partitioning key components of the drivetrain. For example, STMicroelectronics offers the L9907, a smart-power FET driver for three-phase brushless DC motors. It is built in the company’s BCD-6s process and can control six pre-driver channels independently, enabling a variety of motor control strategies for three-phase brushless DC motors.

Elmos has taken a different approach with its E523.52, a programmable, high-voltage brushless motor controller for 24V and 48V vehicles. It has three half-bridge drivers, an 11V DC/DC step-down converter, two linear regulators, and a 16bit microcontroller. The 11V output can power six gate drivers, internal linear regulators, and external loads such as external Hall sensors.

Lower down the integration chain, companies such as Infineon and ON Semiconductor are working on power transistors optimised for 48V automotive applications. Infineon is using its OptiMOS 80V/100V trench technology and leadless TOLL or TOLG packages to build basic devices for 48V applications. ON Semiconductor is introducing a family of very low resistance 80V N-channel PowerTrench MOSFETs in a compact TOLL package, which it says are a good fit for high-current 48V applications.

Panasonic EEh-ZE series hybrid aluminium electrolytic capacitors  

The increased currents and voltages used in 48V systems will inevitably lead to a more electrically noisy environment. Some manufacturers are already working on ways to counter this problem. For example, Panasonic’s EEH-ZE series hybrid aluminium electrolytic capacitors (left) have been designed for use in filtering the inputs and outputs of power converters and voltage regulators, for power and battery decoupling, and in a variety of automotive applications. The parts are surface-mountable and comply with AEC-Q200.

Yageo makes two ranges of multilayer ceramic capacitors for the automotive market. The AC series, NP0/X7R parts are available with working voltages ranging from 6.3V to 630V, and at capacitances ranging from 0.2pF to 2.2mF. They’re designed for a range of automotive applications, including entertainment, comfort, security and infotainment. Importantly, the parts are free of lead and halogens, comply with RoHS requirements, and meet the AEC-Q200 automotive quality standard.

The AS series parts are available in capacitances from 1nF to 4.7uF, and with operating voltages from 10V to 250V. They have similar applications, environmental and quality characteristics to the AC series parts, but have soft terminations made up of multiple layers of plating. The soft terminations act as a form of strain relief, making the parts less likely to crack if the board to which they are soldered is flexed.

The shift to e-mobility is also creating demand for new forms of passives. TDK’s CeraLink capacitors are designed to act as ripple-current suppressors, DC link capacitors, and snubbers in the own generation of fast-switching automotive power supplies and inverters made possible by the availability of new IGBTs and MOSFETs, where low equivalent series resistances and inductances are important.

  Vishay IHLP series inductors

Vishay has developed a range of surface-mountable power inductors for the automotive industry. The IHLP parts (right) are made by forming a copper coil onto a lead frame and then encapsulating it in powdered iron and epoxy. The inductors can withstand operating temperatures of 125°C, have low DC resistance and core loss, are self-shielding, and are smaller and lighter than alternatives.

The shift to 48V, especially at relatively high currents, also demands a shift in the way that a vehicle’s electrical systems are interconnected. Low resistance, sealing, durability, reliability and price are among the factors that should all play a role in informing your choice of connector.

Aptiv is responding to this market opportunity with its PowerPack 1000 line of high-current, highly sealed connectors. They are designed to be compact, easy to assemble, robust against vibrations, with a proven terminal design. The connectors can carry currents of up to 145A at 85C, and will work with cables of 8 to 10sq mm, or 19 to 25sq mm. The operating temperature range is –40°C to +125°C and sealing specs include IP67, IP6K9K and S3. The company suggest the PowerPack 1000 connectors are ideal for use in power distribution boxes, start-stop systems, electric turbos, battery connections, active suspension, and for motor generator units.

Adding a 48V subsystem to today’s vehicles will boost their efficiency and reduce their emissions. It will also the pave the way to future advanced hybrid and fully electric vehicles that bring exciting new features to the world of personal transport. 

Connectors, capacitors, and magnetics play a critical role in the reliability and functionality of these systems, and the market is developing rapidly to meet increasing demands in this space. The choice on offer is substantial, and choosing appropriately is key.Explore Avnet Abacus' automotive solutions from some of the world's leading suppliers, or if you need advice on your design, click the Ask an Expert button to get in touch with one of our technical specialists in your local language.

Want more like this? Sign up for our newsletters

The Shift to 48V in Automotive Systems: What You Need To Know | Engineers' Insight | Avnet Abacus

Display portlet menu
Contact our product specialists

Ask an expert

Have a question? Our regional technical specialists are on hand to help.

The Shift to 48V in Automotive Systems: What You Need To Know | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Articles
Autonomous vehicles communicating with each other on roads
How automotive Ethernet and 5G will power autonomous driving
September 22, 2020
Automotive Ethernet and high-performance 5G communication systems will form the backbone of autonomous vehicles, enabling safety, and increased comfort for drivers and passengers.
An electric vehicle charging cable being plugged into a charging station
An introduction to EV charging infrastructure design
February 7, 2020
With demand for faster charging of EV vehicles increasing, the design of charging stations and infrastructure becomes ever more important.
Inside of a connected car depicting
V2X: The future of vehicle communications
By Martin Keenan   -   December 10, 2019
Vehicles are about to become a lot more communicative: with other road users, with the infrastructure they pass on their journeys, with cloud-based services, and even with the energy grid. This communication should make vehicles more economical to operate...
Tesla plugged into charging station
Switching high voltages and currents with PCB-mounted relays
By Martin Keenan   -   November 8, 2019
The growing demand for safe, robust and energy-efficient ways to switch relatively large amounts of power means that relays have an important role to play in a wide range of modern applications.
While connectors are not the most interesting components in automotive systems, they can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
4 factors steering connector choices in today's automotive applications
September 16, 2019
Connectors are critical components in any automotive systems, and their selection can make or break a design. Here, Mathias Goebel looks at the four main factors affecting connector choices in modern automotive applications.
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
How can combining different types of sensors result in more accurate data?
By Alessandro Mastellari   -   May 9, 2019
With more and more applications combining data from multiple sensors, Alessandro Mastellari looks at how sensor fusion is being applied with pressure sensors.
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
Pressure sensors: Why you should consider going digital
By Martin Keenan   -   May 9, 2019
To give the electronic systems we design the ability to detect changes to what is around them we need analogue sensors. But the processing that sits behind those sensors is in almost every case going to be in the digital domain.
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensor miniaturisation: How smaller sensors are enabling better healthcare
By Alessandro Mastellari   -   May 8, 2019
In the second installment of our pressure sensor series Alessandro Mastellari explores how manufacturers are developing smaller and smaller devices.
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
What the growing pressure sensor market means for electronics
By Martin Keenan   -   May 8, 2019
Pressure sensors became to automotive systems in the early 1990s, but as the rate of adoption of these components increases Martin Keenan investigates why.
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Design trends: Automotive passives
By Martin Keenan   -   November 29, 2018
Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough electronics to get a spark to each plug at the right time. Today’s vehicles are radically more complex.
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
DC-DC power conversion challenges in transportation applications
By Andrew Hutton   -   November 22, 2018
Transportation vehicles pose a challenging environment for the power supply designer. DC-DC converters are used to power on-board sensors, communication radios, positioning and location sensing, lighting, and information systems. Huge voltage variati
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
3 reasons to visit Avnet Abacus at electronica 2018
November 12, 2018
As electronica 2018 prepares to open its doors, here are three reasons you should visit Avnet Abacus on stand C5 101 this week.
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
A supercapacitor in every system? Potential is turning to probability
By Ekaterina Rachel   -   August 24, 2018
Traditional battery technologies are being challenged by a relatively new kid on the block, the supercapacitor, and forcing developers across a range of battery-powered applications to examine just what and when power is needed for their system.
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Identifying ‘hot spots’ before they cause thermal runaway
By Juliette Whithair   -   August 16, 2018
Thermal runaway can happen as a direct result of component failure and cause a lot of damage, but there are ways to protect against it.
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
EV charging points set to rapidly increase in numbers
By Marco Enge   -   January 18, 2018
Numbers of EV charging points are set to increase dramatically under a draft EU directive expected to come into effect in 2019, but the design challenges for EV charging solutions are many and varied.
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
Balancing performance, speed and cost for rugged interconnect technologies
By Martin Keenan   -   November 2, 2017
Connector manufacturers are working hard to enhance the performance of rugged connectors, writes Martin Keenan, Avnet Abacus
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
Automotive telematics become mandatory with eCall
By Alan Jermyn   -   August 1, 2017
As the intelligence of vehicle electronic systems increases, wireless connectivity is becoming an important feature, enabling passenger communications and cloud connectivity for advanced features instances of emergency such as eCall.
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Meeting regulatory requirements for mission-critical and non-mission-critical rolling stock power supplies
By Philip Lechner   -   June 13, 2017
All the electronics in rolling stock is subject to challenging environmental conditions, from high temperatures in confined spaces to the heavy vibration felt by body- or axle-mounted systems. Power supplies are no exception, and must comply with rel
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
Sensor Fusion: The future of intelligent devices
By Martin Keenan   -   March 14, 2017
Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own.
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Second Generation MEMS Enables Impressive Performance for Automotive and Industrial IMUs
By Adam Chidley   -   August 18, 2016
When Murata purchased Finnish MEMS specialist VTI Technologies and renamed it Murata Electronics Oy at the start of 2012, it gained the company’s unique 3D MEMS technology which has outstanding performance and reliability in harsh environments.
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.
Supercapacitors: Making transport more efficient
By Adam Chidley   -   September 7, 2015
Today, supercapacitors are widely used in transport applications to help stabilise the output power of a main power source and improve fuel efficiency.

The Shift to 48V in Automotive Systems: What You Need To Know | Engineers' Insight | Avnet Abacus

Display portlet menu
Related Events