Single Pair Ethernet (SPE) solutions
Single Pair Ethernet (SPE) is a new standard in Ethernet connectivity, enabling intelligent networking and integrated power over a single twisted pair connection.
Ethernet, defined by the IEEE 802.3 Ethernet working group, is one of the most widely used networking standards and is ubiquitous in building, industrial and transportation environments. Since being standardised in 1983 Ethernet has developed to provide reliable high-speed communications and become more prevalent in industrial applications with the arrival of features such as Time Sensitive Networking (TSN) and a wide range of robust industrial connector and cable options. Meanwhile, increasing levels of intelligence and automation are being developed across industrial equipment, leading to large numbers of devices which need to be networked as the Industrial Internet of Things accelerates.
In industrial networks, Ethernet has traditionally not been used at the edge device level where various BUS systems have prevailed e.g. Fieldbus. These legacy systems typically have simpler and lower cost cabling requirements than standard Ethernet, which has a large impact when there are hundreds or thousands of sensors and actuators deployed. However, connecting these edge devices with Ethernet would bring the ability to support higher data rates, remove the need for gateways and protocol translation components in the network and provide more sophisticated networking features such as TSN. Single Pair Ethernet has thus evolved to bring the benefits of Ethernet connectivity in a simplified, lightweight infrastructure that enables mass deployment of the Industrial IoT.
In addition to providing data connectivity with Ethernet, SPE allows supply of power to end devices via Power over Data Line (PoDL), where previously this would require two or four twisted pairs. This will enable new possibilities for reliable, Ethernet connected end devices that require no additional power source via cables or batteries.
Features | Applications | |
|
|
|
Want to learn more? Download our Single Pair Ethernet technical specifications.
DOWNLOAD SPE TECH SPEC
Single Pair Ethernet solutions from TE Connectivity
|
In the past, multiple wires for fast 100Mbps Ethernet and even more wires for Gbps Ethernet were required. Now with Single Pair Ethernet, only two wires are needed for data and power (PoDL, Power over Data Line). This significantly reduces complexity, costs and enables innovation beyond existing borders. TE Connectivity has long been driving innovation in the automotive industry with this smaller, lighter, smarter technology. It is now bringing SPE’s powerful advantages to the infrastructure for the Industrial Internet of Things.
TE Connectivity is also proud to be a founding partner of the SPE Industrial Partner Network. TE and all members are driving this technology to get widely adopted by the industry and promoting IEC 63171-6 as the relevant connector standard for industrial applications.
TE Connectivity works closely with Avnet Abacus technical specialists to provide you with the highest level of support for you design. If you require design support on TE Connectivity products, get in touch with our team in your local language.
Engineering Services
Ask an expert
Have a question about Single Pair Ethernet? Our regional technical specialists are on hand to help

Engineers insight
An introduction to Single Pair Ethernet
Single Pair Ethernet is the perfect power delivery and data networking method for IIoT. Learn why in this introduction to SPE.

Engineering samples
Single Pair Ethernet sample kits
Request a TE Connectivity Single Pair Ethernet (SPE) sample kit to test with your IIoT designs.

TE Connectivity white paper
Higher power levels for Single Pair Ethernet
Discover how Single Pair Ethernet can provide high power levels without affecting the data transmission. This makes it an attractive candidate for networks where the actuators and sensors are mounted directly on machines.

Explainer
Single Pair Ethernet technology
Learn more about Single Pair Ethernet and how TE Connectivity can help you with your IIoT design.

Single Pair Ethernet: tomorrow's technology today
In this webinar, Ruud van den Brink, Product Manager, TE Connectivity, discusses the Single Pair Ethernet technology and TE Connectivity’s solutions to enable you to go beyond existing borders.
Watch webinarSingle Pair Ethernet round table discussion
Experts from TE Connectivity discuss what Single Pair Ethernet is, and what the technology will mean for Industrial IoT infrastructure.
watch webinar