EMEA_Avnet Logistics_Warehouse Locations Title

Display portlet menu

Avnet Logistics locations

Avnet Logistics Poing

Avnet Logistics are specialists in handling electronic components, providing ESD protection and operating quality-management systems based on ISO 9001, EN61340-5-1 & 2, ISO 14001 and J-STD020 & 033.

The Logistic Center in Poing is certified according to EN9120 and demonstrates its conformance to aviation, space and defence industry standards. EN9120 specifies additional management system requirements towards quality, safety and reliability within the supply chain of the Aerospace industry. This includes the chain of custody, traceability, stock control and availability of records.

The warehouse Poing 1 has a total storage area of 27.500m² with 157.000 stock locations in the shelf area and another 12.000 locations in the pallets area.

The warehouse Poing² was built in 2011. The warehouse consists of a total area of 32.000m² (expanded by 7.500m²) with 289.000 storage locations in the shelf area and additional 45.000 locations in the Autostore.

ALS_Warehouse Locations_Autostore

Display portlet menu

The Autostore

The Autostore is a unique worldwide-patented warehouse system proven to be the ideal small-goods handler. With standardised boxes stacked in a cube, it is the most space-efficient goods-to-man system on the market. Besides that, there are 31.000 storage locations in the pallet area. The warehouse also features a sequencer, whose task is to collect all the individual items of orders and shipments, sort, store, save and perform together. The sequencer's performance is far above the current industry standard: twelve independent shuttles in three equally independent lanes allow 1200 called games per lane. Sufficient for each job density and a significant relief for picking.

ALS_Warehouse Location_Tongeren

Display portlet menu

Tongeren (Belgium)

The Tongeren Distribution Center handles interconnect passive and electromechanical (IP&E) products for Avnet Abacus, Avnet Integrated Solutions, MSC Technologies and Avnet Silica organizations supported by following certifications:

  • ISO 9001 (quality management), ISO 14001 (environmental)
  • AS 9120 (aerospace Industries)
  • IEC 61340-5, JESD 625 (protection electronical components)
  • AEO certified (European Customs label)
     

The Tongeren plant is strategically located in an industrial zone in terms of available distribution carrier hubs. It was initially constructed in 1999, expanded in 2008 and reshaped during the course of 2018 and 2019. The outcome is a newly equipped warehouse with a footprint of 25.325 m² and options to expand on adjacent land of 12.000 m².

  • 25.325 m² current warehouse area
  • 15.000 high bay pallet racking locations
  • 220.000 shelf storage locations
  • Operating hours – 6 am to 10 pm
  • Vacuum pick services
  • Tape & reel services
     

The logistic center in Tongeren demonstrates its conformance to aviation, space and defense industry standards such as management system requirements in regards to quality, safety and reliability within the supply chain of the aerospace industry. This includes the chain of custody, traceability, stock control and availability of records.

The organization is characterized by a positive social working climate and a continuous improvement based culture.

 

Avnet Logistics

ESD & Moisture Sensitivity

Virtually all materials, even conductors, can be tribo-electrically charged depending on different factors.

EMEA_Quality Certifications_GBD

Display portlet menu

About Avnet EMEA

Quality information

Avnet Logistics in Europe operates Quality Management Systems in accordance with ISO 9001, EN/AS 9120 and ISO 14001.

About Avnet EMEA

Environmental policy

The economical use of energy and raw materials is a component of our business policy as is the protection of water, ground and air.

EMEA_Careers_Job Openings ALS GB

Display portlet menu

About Avnet EMEA

Job openings at Avnet Logistics

Learn more about how you can further your career with Avnet Logistics