3-use-cases-for-embedded-platforms-enabling-HMIs-and-IoT-systems

Display portlet menu

3-use-cases-for-embedded-platforms-enabling-HMIs-and-IoT-systems

Display portlet menu

3 use cases for embedded platforms enabling HMIs and IoT systems

Sales clerk at retail display
Sales clerk at retail display

The demand for intelligent human machine interface (HMI) systems, flexible panel PCs and easy-to-configure Internet of Things (IoT) gateways for industry remains strong and will continue to grow.

In the development of these innovative industrial products, flexible design and optimized time-to-market are the main priorities. The aim is to bring the new system onto the market quickly in order to secure valuable market share.

The driving forces are modern applications —  diverse visualization and complex display solutions, object recognition systems, IoT gateways, medical devices, professional infotainment systems, building automation systems, transportation applications and gaming systems.

To quickly develop a precisely tailored hardware solution for each application, more and more standardized basic components are being used.

A broad section of predefined, already verified building blocks such as embedded computer modules or connectivity solutions can get designers so far. Combining a standardized computer-on-module (COM) with a standard baseboard can move designs even further.
 

These use cases illustrate some of the outcomes:

Human-machine interaction for fitness equipment
 

2D image of heart rate and chart

Challenges:

  • Eliminate one-time engineering costs
  • Ensure long-term availability of solution
  • Accommodate changing system needs over time

SimpleFlex Solution:

  • Flexible architecture based on ARM or x86 processors
  • Stable platform based on fixed long-term design
  • Adaptable assembly options

Benefits:

  • SimpleFlex provides fast time to market and flexible capacity for change that persists over the long-term lifecycle of the solution.

 

 

Railway passenger information and ticketing system
 

2D image of train on tracks

Challenges:

  • Create carrier board without in-house hardware engineering resources
  • Provide customizations for onboard railway operating environment

SimpleFlex Solution:

  • Ready-to-use SimpleFlex carrier with minor changes
  • Assembly customization to add DIP switches to adjust display settings
  • Configuration of board with locking connectors

Benefits:

  • SimpleFlex drives down non-recurring engineering costs and accelerates time to market.

 

 

Large-format customer-interaction display

2D clipart of hand on touch screen

Challenges:

  • Replace existing solution developed in-house with small LCD and simple microcontroller
  • Meet market expectations for large displays with video and PCAP
  • Produce at low volume (<2000 units per year)

SimpleFlex Solution:

  • Off-the-shelf carrier board, with zero one-time engineering cost
  • Variable design based on ARM or x86 architecture as needed
  • Customization through assembly options

Benefits:

  • SimpleFlex cost-effectively provides fast time to market and variable design at low production volume, with excellent technical support.

 

 

One of the simplest ways to bring this to market is through a semi-prefabricated solution like Avnet Integrated’s SimpleFlex platform. Equipped with the selected SMARC 2.0™ module according to customer-specific requirements, and easily configured without development effort, it ensures high flexibility with more than 30 prevalidated interface combinations and can be combined with all displays and touch screens — including configurable SimplePlus displays — to build a complete HMI system.

Learn more about the benefits of the SimpleFlex platform in our whitepaper, Avoiding 3 major embedded computing challenges.

 

 

3-use-cases-for-embedded-platforms-enabling-HMIs-and-IoT-systems

Display portlet menu

3-use-cases-for-embedded-platforms-enabling-HMIs-and-IoT-systems

Display portlet menu
Related Articles
Marie Curie
AI Inference at the Edge: A lesson from Marie Curie
October 12, 2020
In 1914, Marie Curie’s work on radium stopped in its tracks as the reality of World War I approached. Undaunted, Curie sent her entire stock of radium to a local bank by train and embarked on a new project – using her knowledge of radiology to save soldie...
computer screens
Regulatory insights: Are your computer, audiovisual and information technology products ready for the transition to 62368-1?
May 6, 2020
Regulatory certification can be confusing because of constantly changing standards, the complexity of the process and the amount of time needed to properly complete it.
Person placing a component on a board
Does hardware matter?
By Anatoli Lukkarinen   -   March 3, 2020
I believe every IoT and Industrial IoT system designer and software developer should consider the question in the title. Do you?
Processor laying in water
Two methods gaining steam as data center liquid cooling goes mainstream
By Alp Sezen   -   November 24, 2019
Liquid cooled computers for many years have been associated with gaming PC’s and more recently specialized markets like Bitcoin mining.
Business people around a table in a meeting about IoT security
Customization comes with a competitive edge—and security challenge
By Guillaume Crinon   -   September 7, 2018
Whether you have an in-house team or are exporting the building of infrastructure to a trusted partner, make sure the team is asking the right questions when it comes to implementing and deploying IoT solutions.
supply chain concept with vehicles and tools around the work IoT
For Industry 4.0, Reliability Builds on Robust Connections
June 11, 2017
Looking to relieve increasing product complexity and cost pressures, manufacturers are moving toward the next phase of industrial automation envisioned in Industry 4.0. In this concept, smart factories respond instantly to changing workloads to more
Touch screens
Machines in the middle: infection transmission via touchscreens
June 12, 2020
In the last few months, what we touch – and who else has touched it - has suddenly become a critical thought process that very few people thought of previously. Touch screens, devices, kiosks, fuel pumps – people are a lot more conscious of what they have...
SMARC 2.0 module that was integrated 1:1 as Avnet Integrated
Industrial automation demands high flexibility
By Klaus-Michael Hussmann   -   August 22, 2019
Based on deep expertise and an extensive portfolio of SMARC 2.0, Qseven, COM Express and nanoRISC standard modules, Avnet Integrated offers application-optimized single board computer solutions. These innovative products are designed for industrial a
Woman using machinery to modify a display cover lens
Should you chemically or thermally strengthen your glass display cover lens?
August 20, 2019
Durability and safety considerations require the glass to be strengthened (hardened), using either chemical or thermal processes. Chemical hardening is possible with all glass, while thermal hardening is only available for thicknesses up to 3 mm.
A doctor writing on a clipboard
How AI-powered virtual assistants can transform healthcare
February 26, 2019
We have witnessed a paradigm shift in the way patients are being treated by the doctors with the help of AI and machine learning.
depiction of brain surrounded by icons
The rise of machine intelligence in the AI era
February 26, 2019
Whether you know it or not, this technology has a lot of potential to deal with business-specific challenges and the benefits of deep learning outnumber its drawbacks.
An image of the MSC-6B-CFLH board
Highest computing and graphics performance
February 21, 2019
With the MSC C6B-CFLH, Avnet Integrated delivers an extremely powerful COM Express module based on processors from the 8th Generation Intel Core processor family. The high-end board has up to six CPU cores.
man using tablet computer in industrial setting
5 of the best artificial intelligence use cases
January 3, 2019
AI’s upgraded algorithms make predictive analytics, parse data, and help businesses make smarter decisions from the boardroom to the factory floor.
Doctor checking on a patient from a remote patient monitoring device -- artificial intelligence
AI From A-Z: The biggest buzzwords around artificial intelligence
November 28, 2018
Companies across markets from consumer electronics to factory floors are finding power in the introduction of two letters: AI (artificial intelligence).
Solar panels providing an alternate power source with the city skyline they are powering in the background
Alternative Solutions For Powering IoT Devices
August 9, 2018
In this article, we look at why edge devices need power, and the options for reducing this need to a level where energy harvesting becomes sustainable.
energy harvesting concept with green batteries sprouting from the ground
Powering the Internet of Things via Energy Harvesting
June 11, 2017
The push is on to add Internet capability to everything—often called the Internet of Things (IoT)—and the challenge for design engineers is to figure out how to power each of these IoT nodes.
IoT concept image with icons in cloud bubbles over cityscape
Harnessing the Power of IoT: Microsoft’s Unique Approach
March 30, 2017
Little could this now-famous British serial entrepreneur have known in 1999 that the name he chose to define his approach for using RFID in P&G’s supply chain would top Gartner’s 2015 Hype Cycle for Emerging Technologies report. Hackneyed though

3-use-cases-for-embedded-platforms-enabling-HMIs-and-IoT-systems

Display portlet menu
Related Events

No related events found